Part Number: AMC3336-Q1
Other Parts Discussed in Thread: AMC3336
Tool/software:
Good afternoon,
I am using AMC3336-Q1 to measure a motor controller DC input bus (range 0-1000VDC). While the motor controller is operating at 20-30% of maximum current (I_Max = 150Apk), AMC3336 "locks" up:
- Achievable range is reported. In this case 1282.9V is reported which is equivalent to ~30,518 counts.
- DIAG line is set to 1
- Overvoltage trip is triggered
The only way to recover is to completely cycle power. After a power cycle, IC goes back to normal operation.
DIAG line can be set to 1 due to:
- Power brown out
- I took a measurement between pin 3 and 8 and at the switching frequency(40kHz) voltage is ringing between 4.3 and 2.3VDC
- A lack of data between modulator on HV side and Digital interface on LV side of IC
Data locking is a behavior that I have never observed before on these parts.
Here is the schematic
Thank you for any assistance!