Other Parts Discussed in Thread: DAC38J84
Tool/software:
Hello TI Support,
I am working on a system consists of off the shelf board using Xilinx ZU29DR RFSOC paired with Abaco FMC216 with TI DAC39J84 DACs.
The issue I am currently having is that I could not get any output from the DACs.
My Configuration (Sequencing based on TI "1323.8.3 DAC3xJ8x Start-up Sequence.docx"):
- JESD204B Subclass-1 in 2441 configuration (L=2, M=4, F=4, S=1)
- 32 frames/multi-frame (i.e. K = 32)
- SerDes Line Rate 9.8304 Gbps, w/ interpolation of 8x
- DAC config (File attached also)
- DACCLKP/N = 491.52 MHz from LMK04828B
- Register configs (All values in decimal)
- Config51: pll_vcosel = 1 (L-Band 4 GHz)
- Config51: pll_vco = 17
- Config50: pll_p = 0
- Config50: pll_m = 15
- Config49: pll_n = 3
- Config59: serdes_clk_sel = 0 (DACCLKP/N)
- Config59: serdes_refclk_div = 0
- Config60: rw_cfgpll = 20 (i.e. 5x)
- Config62: rw_cfgrx0 = 0 (Full rate)
- Config37: clkjesd_div = 2
- DACCLK (DAC PLL block output) = 1966.08 MHz
- SerDes PLL: 2457.6 MHz
- REFCLK for SerDes PLL: 491.52 MHz
- JESDclk: 491.52 MHz
- SysRef: Continuous 7.68 MHz from LMK04828B
- One Xilinx JESD Core + Xilinx JESD Phy connected to one DAC39J84 IC (1 Link, 2 Lanes)
- Xilinx JESD Core Clock 245.76 MHz
- LMK04828B Reference clock: 122.88 MHz
- DAC samples formatted in MSB first before transmission
What I've confirmed
- CGS completed successfully without errors/alarms
- ILA completed successfully without errors/alarms
- SYNCB line is toggled at expected times (i.e. Before CGS starts, after CGS completes). No lane reinitialization due to link errors observed upon successful link initialization; i.e. Link is stable
- SYSREF frequency is 7.68 MHz (measured on scope)
- PASSED NCO tests (per TI "7534.SYSREF trouble-shooting.docx") for ALL DACS and DAC channels
- Confirmed Xilinx JESD Core implementation is transmitting DAC samples in MSB then LSB format.
- No errors/alarms reported on Lane0 and Lane1 on the DAC (i.e. Config65, Config100, Config101, Config108)
- No errors reported on the Xilinx JESD Core (i.e. STAT_STATUS Register 0x60, STAT_LINK_ERR_CNT Register 0x420/0x4A0)
I have been struggling on this "No DAC output" problem for many weeks now.
Any help you can provide is greatly appreciated.
TI references used:
- 4188.DAC38J84 Clock, PLL and SERDES Configuration.docx
- 1323.8.3 DAC3xJ8x Start-up Sequence.docx
- 7534.SYSREF trouble-shooting.docx
Dumping DAC 0 Register values DAC 0 Register: 0x00 (0) Value: 0x0418 (0000 0100 0001 1000b) DAC 0 Register: 0x01 (1) Value: 0x00a0 (0000 0000 1010 0000b) DAC 0 Register: 0x02 (2) Value: 0x2082 (0010 0000 1000 0010b) DAC 0 Register: 0x03 (3) Value: 0xa300 (1010 0011 0000 0000b) DAC 0 Register: 0x04 (4) Value: 0xfcfc (1111 1100 1111 1100b) DAC 0 Register: 0x05 (5) Value: 0xef06 (1110 1111 0000 0110b) DAC 0 Register: 0x06 (6) Value: 0xfcfc (1111 1100 1111 1100b) DAC 0 Register: 0x07 (7) Value: 0x3701 (0011 0111 0000 0001b) DAC 0 Register: 0x08 (8) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x09 (9) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x0a (10) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x0b (11) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x0c (12) Value: 0x0400 (0000 0100 0000 0000b) DAC 0 Register: 0x0d (13) Value: 0x0400 (0000 0100 0000 0000b) DAC 0 Register: 0x0e (14) Value: 0x0400 (0000 0100 0000 0000b) DAC 0 Register: 0x0f (15) Value: 0x0400 (0000 0100 0000 0000b) DAC 0 Register: 0x10 (16) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x11 (17) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x12 (18) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x13 (19) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x14 (20) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x15 (21) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x16 (22) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x17 (23) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x18 (24) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x19 (25) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x1a (26) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x1b (27) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x1c (28) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x1d (29) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x1e (30) Value: 0x4444 (0100 0100 0100 0100b) DAC 0 Register: 0x1f (31) Value: 0x4440 (0100 0100 0100 0000b) DAC 0 Register: 0x20 (32) Value: 0x4044 (0100 0000 0100 0100b) DAC 0 Register: 0x21 (33) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x22 (34) Value: 0x1b1b (0001 1011 0001 1011b) DAC 0 Register: 0x23 (35) Value: 0xffbf (1111 1111 1011 1111b) DAC 0 Register: 0x24 (36) Value: 0x0030 (0000 0000 0011 0000b) DAC 0 Register: 0x25 (37) Value: 0x4000 (0100 0000 0000 0000b) DAC 0 Register: 0x26 (38) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x27 (39) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x28 (40) Value: 0x0003 (0000 0000 0000 0011b) DAC 0 Register: 0x29 (41) Value: 0xffff (1111 1111 1111 1111b) DAC 0 Register: 0x2a (42) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x2b (43) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x2c (44) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x2d (45) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x2e (46) Value: 0xffff (1111 1111 1111 1111b) DAC 0 Register: 0x2f (47) Value: 0x0004 (0000 0000 0000 0100b) DAC 0 Register: 0x30 (48) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x31 (49) Value: 0x641c (0110 0100 0001 1100b) DAC 0 Register: 0x32 (50) Value: 0x0f00 (0000 1111 0000 0000b) DAC 0 Register: 0x33 (51) Value: 0xa37c (1010 0011 0111 1100b) DAC 0 Register: 0x34 (52) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x35 (53) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x36 (54) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x37 (55) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x38 (56) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x39 (57) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x3a (58) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x3b (59) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x3c (60) Value: 0x1028 (0001 0000 0010 1000b) DAC 0 Register: 0x3d (61) Value: 0x0088 (0000 0000 1000 1000b) DAC 0 Register: 0x3e (62) Value: 0x0108 (0000 0001 0000 1000b) DAC 0 Register: 0x3f (63) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x40 (64) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x41 (65) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x42 (66) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x43 (67) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x44 (68) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x45 (69) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x46 (70) Value: 0x0044 (0000 0000 0100 0100b) DAC 0 Register: 0x47 (71) Value: 0x190a (0001 1001 0000 1010b) DAC 0 Register: 0x48 (72) Value: 0x31c3 (0011 0001 1100 0011b) DAC 0 Register: 0x49 (73) Value: 0x5500 (0101 0101 0000 0000b) DAC 0 Register: 0x4a (74) Value: 0x0301 (0000 0011 0000 0001b) DAC 0 Register: 0x4b (75) Value: 0x1c03 (0001 1100 0000 0011b) DAC 0 Register: 0x4c (76) Value: 0x1f01 (0001 1111 0000 0001b) DAC 0 Register: 0x4d (77) Value: 0x0300 (0000 0011 0000 0000b) DAC 0 Register: 0x4e (78) Value: 0x0f0f (0000 1111 0000 1111b) DAC 0 Register: 0x4f (79) Value: 0x1cc1 (0001 1100 1100 0001b) DAC 0 Register: 0x50 (80) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x51 (81) Value: 0x00ff (0000 0000 1111 1111b) DAC 0 Register: 0x52 (82) Value: 0x00ff (0000 0000 1111 1111b) DAC 0 Register: 0x53 (83) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x54 (84) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x55 (85) Value: 0x00ff (0000 0000 1111 1111b) DAC 0 Register: 0x56 (86) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x57 (87) Value: 0x00ff (0000 0000 1111 1111b) DAC 0 Register: 0x58 (88) Value: 0x00ff (0000 0000 1111 1111b) DAC 0 Register: 0x59 (89) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x5a (90) Value: 0x00ff (0000 0000 1111 1111b) DAC 0 Register: 0x5b (91) Value: 0x00ff (0000 0000 1111 1111b) DAC 0 Register: 0x5c (92) Value: 0x1115 (0001 0001 0001 0101b) DAC 0 Register: 0x5d (93) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x5e (94) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x5f (95) Value: 0x0123 (0000 0001 0010 0011b) DAC 0 Register: 0x60 (96) Value: 0x4567 (0100 0101 0110 0111b) DAC 0 Register: 0x61 (97) Value: 0x0001 (0000 0000 0000 0001b) DAC 0 Register: 0x62 (98) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x63 (99) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x64 (100) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x65 (101) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x66 (102) Value: 0xb00a (1011 0000 0000 1010b) DAC 0 Register: 0x67 (103) Value: 0xef0b (1110 1111 0000 1011b) DAC 0 Register: 0x68 (104) Value: 0xce06 (1100 1110 0000 0110b) DAC 0 Register: 0x69 (105) Value: 0x7507 (0111 0101 0000 0111b) DAC 0 Register: 0x6a (106) Value: 0x220e (0010 0010 0000 1110b) DAC 0 Register: 0x6b (107) Value: 0xf60f (1111 0110 0000 1111b) DAC 0 Register: 0x6c (108) Value: 0x0006 (0000 0000 0000 0110b) DAC 0 Register: 0x6d (109) Value: 0x00e0 (0000 0000 1110 0000b) DAC 0 Register: 0x6e (110) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x6f (111) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x70 (112) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x71 (113) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x72 (114) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x73 (115) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x74 (116) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x75 (117) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x76 (118) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x77 (119) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x78 (120) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x79 (121) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x7a (122) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x7b (123) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x7c (124) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x7d (125) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x7e (126) Value: 0x0000 (0000 0000 0000 0000b) DAC 0 Register: 0x7f (127) Value: 0x800a (1000 0000 0000 1010b) DAC 0 Register: 0x80 (128) Value: 0x0418 (0000 0100 0001 1000b) Script Completed: 2025-07-24 11:08:29.333475 CommClientSocket destroyed