Part Number: ADC3444
Tool/software:
Hello,
We are working with a custom board that integrates multiple ADC3444 chips. These ADCs are grouped such that half of the chips receive their sampling clock from one HMC7044 clock generator, while the other half are connected to a second HMC7044. Both HMC7044 devices receive a common reference clock input, ensuring their outputs are derived from the same frequency reference.
The ADC3444 chips operate at a sampling rate of 122.88 MHz, and this sampling clock is directly generated by the HMC7044s without using any internal dividers in the ADCs.
We’ve observed that the phase relationship between channels across the ADCs is not preserved across power cycles.
Could this behavior be caused by clock input alignment issues to the ADC3444s? Is there a recommended approach for achieving deterministic multi-chip synchronization in such a setup? We understand that SYSREF may not apply here, as no internal clock dividers are used within the ADCs.
Best regards