Other Parts Discussed in Thread: DAC81001, DAC91001, DAC11001A, REF6250
Tool/software:
The BP-DAC11001EVM User's Guide (SLAU806) indicates that when Jumper J20 is set to position 1-2 (REF_PWR from VCC), VCC should be less than 6V. However, the DAC11001A, DAC91001, DAC81001 datasheet (SLASEL0B) states that the minimum recommended VCC (analog positive power supply) for the DAC chip is 8V. Could you please clarify how the onboard Vref generator (REF6250) is intended to be powered in conjunction with the DAC, given that the DAC's minimum VCC requirement conflicts with the 6V limit specified for the J20 (1-2) jumper option when powering the reference from VCC?