This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC61416:Inquiry about Settling Time (MAX values)

In the datasheet, I found only the typical settling time value (12 μs) for an output range of ±10V. However, there is no information regarding the maximum settling time value. Also, I could not find any settling time values (typical or maximum) for output ranges of ±2.5V and ±5V.

Could you please provide the maximum settling time values for the following output ranges?

  • ±2.5V
  • ±5V
  • ±10V
  • Hi,

    We doesn't have characterisation data for the max settling time value. All i can help here is with typical numbers for ±10V span as mentioned in the data sheet.

    Now coming to the  ±2.5V and ±5V typical settling numbers - it will be less than 12μs as settling has two major constituents a. slew and final settling. And for the lower voltage spans slew time will be lower.

    For your reference, please have a look into one of the it's newer variant device DAC81404.

    Thanks,
    Sanjay