This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDC3256: Multiple gate integration with DDC3256

Part Number: DDC3256

Tool/software:

I would like to use  DDC3256 in combination with the  DDC3256EVM to measure the current coming from an array of photodiodes. The current coming from the photodiodes is very small and I would like to know if I could accumulate in the integrator several exposures of 1.6ms (or of other duration) before doing the analog to digital conversion, and if this is supported by the firmware provided with the DDC3256EVM. So essentially, adding several integrations in the capacitor without resetting it in between diode exposures.