Tool/software:
Hello.
We use the ADS1148 in a number of our products (10k - 100k PA) and are seeing noticeably noisy conversion results in approximately 2% of our units.
The ADS1148 is connected to an LPC812 MCU, and the SPI clock is running at 960kHz.
There is no external main clock to the ADC.
We have configured the ADC to run at 1000 samples per second.
Conversions:
T0: We write a new value to the MUX
T + 500us We use a "read once" strategy over SPI (0x12),(0xFF),(0xFF) and transfer back the result on 2nd and 3rd Bytes.
T + 1ms Write the next value to the MUX...
We are looking for information on how slow / fast the SPI clock can be. The data sheet says minimum period of 488ns, maximum period of 64 conversions.
Does this mean an upper limit of 2.049MHz, and a lower limit of, say, 64ms?
Thank you for clarifications.