Tool/software:
Hello,
What is the input impedance of AINP and AINN when the input buffers are on?
I see in the datasheet (Section 5.5) that there is 2uA input current for Vref = 4.096V, but I'm assuming different input voltages affect input current. My closest working guess is that R_in = Vref/2uA = 2MOhm but I'd like some confirmation if there is an upper or lower bound documented from internal testing.
Thanks,
Dylan