We have been using IC555 in one of our application where in PCB is moulded with the Araldite, since unit is fully immersed in ATF (Aircraft Turbine Fuel) hence moulding is essential to protect electronics to come in contact directly with ATF. In view of above it is requested to kindly confirm that IC 555 can be moulded with the Araldite. In case, if araldite is not suitable then can you please suggest suitable material for moulding which is ATF resistant also? We shall be gratefully if you could kindly give your comments on the above at the earliest.
Regards,