This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0104E: using a 5V SPI waveform output from the MCU to the B end of the chip TXS0104EPWR. I hope the A end can output a 3.3V waveform

Part Number: TXS0104E


Tool/software:

Hello, I'm using a 5V SPI waveform output from the MCU to the B end of the chip TXS0104EPWR. I hope the A end can output a 3.3V waveform. However, when I designed it as follows, I found no waveform output. Could you please help me check which side has the problem?