Part Number: DAC8564
Tool/software:
I am having trouble with my DAC8564, which is generating heat of just under 100 degrees Celsius.
I suspect that the cause is the 3rd pin.
Currently, I have four DAC8564s on a PCB set on a raspberry pi 5, controlling pneumatic valves.
Since the pneumatic valve operates at 0-5V, I have designed the PCB so that the 5V from the raspberry pi 5 is connected to the 3rd pin of the DAC8564 as an external reference.
However, the datasheet of DAC8564 says “If you want to use the external reference, send the command to disable the internal reference to DAC8564 before connecting the external reference”.
Since my PCB have the conncection of the 5V of the raspberry pi5 and the 3rd pin of the DAC8564, this means that I have connected the external reference before sending the command to disable the internal reference to the DAC8564.
I wonder if the collision between the output of the internal reference from the DAC8564 and the input of the external reference is leading to the high heat generation.
Please tell me what behavior DAC8564 does when an external reference is input to pin 3 without sending a command to disable the internal reference.
AVDD is correctly connected to 5V.