This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3644: DC Offset temination loading

Part Number: ADC3644

Tool/software:

Hello, I have designed a fully differential amplifier that has an output termination equivalent to that as seen in section 8.3.1.2.3.1 (AC-coupled) of the datasheet. Disconnected, Vcm is ~900mV, however, once connected as shown in figure 8.7 of the datasheet the voltage appears to drop to ~525mV. Is this a problem with a solution? Thanks.