Part Number: ADS8167
Other Parts Discussed in Thread: REF2041
Tool/software:
Dear TI Support Team,
We are using ADS8167IRHBT devices in one of our ongoing projects. Our system consists of a Power Board and several other functional boards.
Observation:
On the Power Board, the ADS8167 devices operate without any issue. For example, when monitoring the REFBY2 pin through an analog input channel, the measured value remains stable at ~2.048 V, with only a few mV variation. Also, inputs expected to be at 0 V are read by the MCU as ~7–8 mV.
However, on another board which receives its power and ground connections from the Power Board, we observe significant instability on the ADS8167 devices, even though the same schematic and layout have been applied. When REFBY2 is read over SPI, it fluctuates continuously. Based on the software monitoring graph, the value drops rapidly from ~2.048 V down to ~0.4 V and then returns back. In addition, inputs expected to be at 0 V show readings in the range of 300–800 mV, and sometimes even higher.
Additional Information:
All ADCs are supplied with an external 4.096 V reference (REF2041).
Decoupling capacitors are placed very close to the pins in accordance with the datasheet recommendations (REFP–REFM: 22 µF, REFBY2 and REFIO: 1 µF, VDD: 1 µF).
The problematic PCB is 14-layer, with 4 dedicated GND planes, and power/ground is distributed strongly through multiple pins.
The same topology works stably on the Power Board, but REFBY2 and input readings are unstable on the other board.
We have investigated this issue but have not yet reached a clear conclusion. We would greatly appreciate your technical feedback and guidance. Our schematic is also attached below.

Best regards,
Erhan Kızar