Part Number: DAC60508
Tool/software:
Hi,
I want to work with voltage output of 5V with VDD of 5V.
The VDD is not promised to be over 5V and could be a bit under this value (could be 4.75V).
what is the value the reference divider issues a reference alarm condition and set the output to zero?
I didn't have a problem to work with the range of 0V to VDD if VDD is above 4.75V.
Pls. advise
Zeev Gerber