This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC60508: drive multiple dac's (dac60508) with external reference

Part Number: DAC60508
Other Parts Discussed in Thread: TLV431

Tool/software:

Hi,

I want to drive multiple (4) dac's (dac60508) with one voltage reference (tlv431).

the dac60508 drive the reference as output when working with internal reference which is the default.

how to handle the voltage contention between the dac's and the external reference and between the dac's also, until I configure the dac's to work with external reference?

in earlier question, I see TI recommended on series resistor between the reference of ~100ohm.

should i use 4 resistors in this case? one per dac reference pin?

Zeev gerber