This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE5809EVM: Automatic Data Collection

Part Number: AFE5809EVM

Tool/software:

Hello! I'm using AFE5809EVM with TSW1400 to capture data automatically by the external trigger events, but it takes a long time to store data on PC after every event and it spreads the events in time. 
I use my Python-based script with HSDC Pro Automation DLL and High Speed Data Converter Pro v5.0, and when I tried to use "ADC_Auto_ReArm_Trigger_Settings" fuction I got an error, because there weren't such function in my version of DLL.

Is there a way to store data automatically (with ReArm functionality) or at least re-arm the trigger manually to collect couple of trigger-recorded frames? If not, which setup with at least 8 analog input channels, around 50MHz data rate and data capture board with couple frames functionality I can find?