Part Number: DAC63001
Tool/software:
Hello,
I am using DAC63001 as voltage-controlled source for DC/DC converter controller.
What is limitation of current sink/source capability of built in buffer inside of module when DAC is configured as voltage source, not current source?
My application will only require +/-2mA (source/sink) to drive DC/DC converter (feedback voltage), but I need to be able to sustain certain range of voltage but also current as well.
It seems like it's capable of short circuit current up to 10's mA but i'm not sure If I can use this as nominal condition rating.
Thanks