This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0104E: 1.8 V to 3.3 V I2C translation

Part Number: TXS0104E
Other Parts Discussed in Thread: TXS0104V

Tool/software:

This level shifter has been marked as an "SPIO"-application product in TI's website. Currently, I am using two of its channels for UART RX and TX lines. I have two more free channels which I intend to use for my I2C SCL and SDA lines. However, there is TXS0104V - product displaying similar features, but has been marked as an "I2C, MDIO, SMBus, SPIO"-application product. I am not sure if I should go ahead with the IC I already have used earlier or should I go for the second one which is marked for I2C application.