Part Number: ADS8588SEVM-PDK
Other Parts Discussed in Thread: TMDS64EVM, ADC-PHI-PRU-EVM, , SYSCONFIG, ADS8588S, ADS8588H
Tool/software:
Hello!
I try to build the pru io example with TMDS64EVM and ADS8588SEVM-PDK connected with ADC-PHI-PRU-EVM
The example is provided in the AM64x MCU+ SDK 11.01.00.
- When using CCS projects to build, import the CCS project from the above mentioned Example folder path for system_freertos_prufw (It will automatically import R5F and PRU project) for the required combination.
- On importing the project, SysConfig will contain an ADC Config instance with default configurations which are compatible with the ADC-PHI-PRU-EVM Adapter Board, Use R5F SysConfig to configure the required settings for the ADC IC.
Therefore, I attempted to modify the SysConfig via the PADC GUI, but ADS8588S is not an option; only ADS8588H exists. I am using ADS8588S. Is it acceptable to select ADS8588H and proceed?
Or can I access SysConfig without using the GUI?
Below is the link to the SDK documentation containing the relevant example.
software-dl.ti.com/.../EXAMPLES_PRU_ADC_ADS85x8.html