This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS124S06: Are ADS124S06 and ADS114S06 compatible for register map and DC / AC specs?

Part Number: ADS124S06
Other Parts Discussed in Thread: ADS114S06,

Tool/software:

Hi,

Are ADS124S06 and ADS114S06 compatible for register map and DC / AC spcecs etc on datasheet?

I alredy use ADS124S06 (24bit) and develop software on MCU.

If I use ADS114S06(16bit), Can I use same register map and DC / AC specs like ?

Offcource, ADC data is differenct like 16bit and 24bit. Other specs are same , it is easy to move from ADS124S06 to ADS114S06

Best Regards,

ttd

  • Hi ttd,

    Yes, ADS124S06 and ADS114S06 are the functionally and parametrically the same, so you should be able to switch to the 16-bit ADC with very little effort. The main difference is the resolution, and therefore the ADC noise (refer to section 8.1)

    -Bryan