ADS131A04: Is ADS131A04 possible to use for load cell (Bridge Sensor) application.

Part Number: ADS131A04
Other Parts Discussed in Thread: ADS1235

Tool/software:

Dear Specialists,

My customer is considering ADS131A04 for load cell(Bridge Sensor) application and has a question.

I would be grateful if you could advise.

---Questions

Can a simultaneous sampling ΔΣ ADC (ADS131A04) be used for load cells?

The datasheet states that its main use is as a power meter.

From the perspective of load cells, my considerations are as follows:

- The AD converter has good noise characteristics.

- The gain is digital rather than PGA, so external amplification is required.

- The offset drift is large, but this is not a problem as the effect of the external amplifier is dominant.

- An external reference input is possible, so a ratiometric configuration is possible.

- The output rate is fast, but this is not a problem as digital filtering is performed by the microcontroller.

Please let me know if there are any points I should be aware of.

Could you please provide any reference designs or reference materials you have?

---

I appreciate your great help in advance.

Best regards,

Shinichi