This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3543: Using single ended clock. Trouble getting part configured and data output

Part Number: ADC3543
Other Parts Discussed in Thread: CDCV304

Tool/software:

I am bringing up a custom board that uses the ADC3543 data converter. For this application I have elected to go with a single ended clock and I am having difficulties getting the ADC to output data. However, I did get signs of life from the chip: I have intermittently successfully got the chip to output data and I am able to read back the registers I have set using SPI.

Following section 8.3.2.1 in the datasheet I have provided a 50MHz clock (see attached oscilloscope trace) to the  CLKP pin and I connected a 0.1uF capacitor (I also tried a 50pF value with even less success) to the CLKM pin. See attached schematic for details but note that I originally inverted CLKP and CLKM but fixed it with a bodge.

To configure the ADC I started by following table 8-14 in the datasheet and connected the REFBUF pin to ground to select internal reference, single ended clock input and serial CMOS 2-wire. However, looking at figure 8-16 made me think that there is no way that REFBUF can be shorted to ground without shorting out the internal reference (indeed it seems like connecting it to any voltage would short the internal reference). Hence, I cut the trace running to REFBUF... 

Seemingly that meant that I now needed to adjust the clock setting using SPI. According to the datasheet this is register 0x0E which I set to 0b00001001 (setting REF CTL to 1, REF SEL to 00 for internal, and SE CLK EN to 1 for singled ended clock input). Out of an abundance of caution I read the register back to confirm that it was accepted (see oscilloscope trace of transaction). I have tried to touch other registers but I did not seem to help my case as I am still attempting to just see signs of life in a parallel CMOS mode rather than configure the part for my application.

For a short moment in time this made the part work... (REFBUF floating, 0.1uF on CLKM, single command to 0x0E) before the part went between working and not working.... I suspect that this was cased by a bit of water left over from washing adding a tiny bit of resistance somewhere and then evaporating to leave the part in a broken state.... I seek advice on what is wrong with my application. To this end I have attached both the schematic and a screenshot of the layout.

The relevant part of the schematic is attached here. Note that I have bodged the error where the clock was being fed to CLKM instead of CLKP, I have replaced the 47pF capacitor with a 0.1uF and I have cut the trace running to REFBUF.

 tdm_col_adc_forum.pdf

The layout is on a 4 layer board. I am showing the top and first inner layer with the split ground planes

Next is the trace showing that write and the read from the register

Finally a trace of the reasonably decent looking clock. This is being fed to the 

The major "symptom" is that there is no data coming out of the ADC (no clock on DCLK, it appears to be in a high-Z state). I also noticed that the VREF pin is not at 1.6V, might this be caused by me damaging the internal reference by shorting REFBUF to ground? But the Vcm is at 0.95V and the SPI part of the chip appears to be working as shown in the above scope traces.

Please advise,

Simon

P.S. I will note that the datasheet and user experience of this chip has thus far not been comparable with that I have come to expect from the other TI documentation. I hope that since this product is rather new, the datasheet may be updated in the future to improve the user experience with what otherwise seems like an excellent product...

  • Hi Simon,

    If the ADC device was working before, what has changed?

    If the ADC is of suspect, then I would replace it and see if you can get your board working again.

    Regards,

    Rob

  • I think when it momentarily worked there was a few bad solder joints that may have gotten "fixed" with flux residue. I have since reflowed the board and confirmed the joints are good with a microscope. I wouldn't read into it momentarily working - I could have hallucinated it from spending too much time in the lab (joking of course but I think we should focus on the problem at hand). 

    The symptoms are as described above (but the bad solder joint was on the VREF pin so that is fixed). The chip appears to show signs of life:

    When configuring the VREF over SPI it shows up on the VREF pin and when configuring the clock to be single ended it disconnects the 0.9Vcm bias from the unused clock pin. In addition to SPI reading back correctly this to me screams that everything is working as expected. However there is still no data output.

    Is it possible that I am doing something sufficiently incorrect in the register settings? Can you provide what register writes I need to do for a minimal viable CMOS parallel SDR output, internal reference, single ended clock (default bit mapping, no down-converting/filtering/mixing)

    Best,

    Simon

  • Hi Simon,

    It might be easier for you to send us your reg config first and I can test in the lab.

    Please also send sampling rate, I assume you are using 2 wire for the digital config?

    And just to confirm, you are using a single ended input clock config?

    One thought, what are you using to drive the sampling clock on your board?

    Regardless, I see it is not DC blocked, I would put a series 0.1uF cap inline with your clock connection.

    The clock swing could be good, but the common mode voltage might be off.

    Try that too and let me know.

    Thanks,

    Rob

  • Hi Rob, Thank you for your prompt replies.

    As you can see in the screenshot of the scope. I am using a 50MHz single ended clock to drive the sampling rate. I am indeed using the SPI config and I am setting registers successfully. register reads appear correct. I can attach a scope trace of the SPI transaction if you would like but I am fairly confident that the two wire config interface is working correctly

    I have attempted setting register 0x0E to value 0b00001001, that is REF CTL set to 1, REF SEL set to 00 for internal reference, and SE CLK EN 1 for single ended clock. I can attach the C "psudo" code for my initialization.

    I am driving the clock with a CDCV304 and a voltage divider to bring it down to 1.8 logic level. See original post for a scope trace of the clock probed near the ADC. Putting a series 0.1uF is an interesting idea, although the datasheet explicitly shows the direct connection in section 8.3.2.1. 

    I am attaching the initialization code.

    void video_adc_init()
    {
        sleep_ms(100); // wait for the ADC to power up
        // clock idle low -> CPOL_0
        // data sampled on rising edge -> CPHA_0
        // MSB first -> MSB_FIRST
        // 8 bits per word -> 8
        spi_set_format(LOCAL_SPI_PERIPHERAL, 8, SPI_CPOL_0, SPI_CPHA_0, SPI_MSB_FIRST);
    
        // starting with a reset is prudent
        //  write a 1 to bit 0 of register 0x00 to reset the ADC
        write_video_adc(0x00, 0b00000001); // reset the ADC
        sleep_ms(1);
    
        // Register 0x07 has bits 7-5 OP IF MAPPER need to be set to 110 for SDR
        // bit 4 must be set to 0
        // bit 3 is OP IF EN (enables changing the default interface mode ) write 1
        // bit 2-0 are OP IF SEN select output interface set 000 for SDR CMOS
        write_video_adc(0x07, 0b11001000);
        sleep_us(10);
    
    
        // now load config from efuses
        // register 0x13 bit 0 set 1
        write_video_adc(0x13, 0b00000001); // set to load config from efuses
        sleep_ms(2);                       // wait for the ADC to load the config from efuses
        write_video_adc(0x13, 0b00000000); // clear the load config bit
        sleep_us(10);
    
        // write power down stuff for SDR CMOS
        write_video_adc(0x0A, 0x60);
        sleep_us(10);
        write_video_adc(0x0B, 0x1E);
        sleep_us(10);
        write_video_adc(0x0C, 0x0C);
        sleep_us(10);
    
        //power down DCLKIN
        write_video_adc(0x18, 0x00);
        sleep_us(10);
    
        //note that flow chart wants 0x19 to be written to possibly
        //contains FCLK config (used in decimation)
    
        //setup the bit mapper to be off...
        write_video_adc(0x1B, 0x00);
        sleep_us(10);
    
        //enable DCLK
        write_video_adc(0x1F, 0b00010000);
        sleep_us(10);
    
        //this is where one might adjust soemthing about FCLK and duty cycle in 0x20..2
    
        //now one might adjust the bitmaper in 0x39..72
    
        //disable the DDC and enable bypass
        write_video_adc(0x24, 0x00);
        sleep_us(10);
    
        //we can now configure the decimation in 0x25
    
        //can program NCO here in 0x2A..D
    
        //configure complex stuff in 0x27
    
        // set mixer gain in 0x26
    
        //The flowchart in the datasheet ends here. Looking at the remaining registers that have not yet been adjusted...
    
        //power down controls
        //bit 5 turns off clock buffer can make power come back
        write_video_adc(0x08, 0b00000010);
        sleep_us(10);
        //0x0D does power down mask (what the power down pin turns off) ignored
    
        //setup the voltage reference and clock mod 0x0E
        // bit 7-5 control sync (we dont really care about this)
        // bit 4 must be 0
        // bit 3 write 1 to set ref and clk using spi
        // bit 2-1 ref sel write 00 for internal ref
        // bit 0 write 1 for single ended clock
        write_video_adc(0x0E, 0b00001001); // set to internal ref and single ended clock
        sleep_us(10);
    
        // configure the ADC input, set differential and DLL PDN
        write_video_adc(0x11, 0x00);
        sleep_us(10);
    
        //turn off test pattern
        write_video_adc(0x14, 0x00);
        sleep_us(10);
        write_video_adc(0x15, 0x00);
        sleep_us(10);
        write_video_adc(0x16, 0x00);
        sleep_us(10);
    
        //set the DCLK output delay
        write_video_adc(0x1E, 0x00);
    
        sleep_us(100);
    
        // This function reads all the registers one by one and I have scoped them and confirmed that have all taken the expected values.
        read_all();
    
    }
    

    As a higher level question. Do I need to do any configuration to see signs of life from this chip? Should it not just output data as soon as a clock is seen on the input regardless of what configuration I put in? What can cause my symptoms of no data but SPI signs of life?

  • HI Simon,

    Please answer my questions above about the clock and provide the register writes performed.

    Yes, the ADC should show signs of life when the power is brought up.

    Which leads me to think you have a bad ADC if you had shorted leads and powered the device on as mentioned at the start.

    It would be best to start with a fresh ADC or board. 

    Regards,

    Rob

  • Thank you Rob,

    Yes I am starting to suspect the chip. I guess I have done enough due diligence to justify swapping it now. I have one on order and will update when it arrives.

    As I said above:

    • The sampling rate is 50MHz.
    • I am using 2 wire config with 100kBit/s data rate.
    • I am using single ended clock config. 
    • Clock is driven by CDCV304 and a voltage divider to bring it down to 1.8 logic level

    I attempted your suggestion of AC coupling the clock but sadly it did not help my issue. 

    While I wait for the new parts to arrive can you look at my register configs...

    wait 100ms
    0x00, 0b00000001
    wait 1ms
    0x07, 0b11001000
    0x13, 0b00000001
    wait 2ms
    0x13, 0b00000000
    0x0A, 0x60
    0x0B, 0x1E
    0x0C, 0x0C
    0x18, 0x00
    0x1B, 0x00
    0x1F, 0b00010000
    0x24, 0x00
    0x08, 0b00000010
    0x0E, 0b00001001
    0x11, 0x00
    0x14, 0x00
    0x15, 0x00
    0x16, 0x00
    0x1E, 0x00
    wait 100us

    Thank you,

    Simon

  • Hi Simon,

    So you put a 0.1uF series DC blocking cap between the CDC device and the ADC?

    Can you measure the common mode DC voltage on the clock pin you are driving? It should be around 0.9VDC.

    Might be good to draw out for me what is actually being connect as a clock to the ADC, basically on what was done and what you are doing now?

    If you put too big a signal swing into the ADC clock pin, you likely destroyed that input, and would never get a clock into the ADC.

    And therefore, never get any digital outputs to toggle.

    Thanks,

    Rob

  • Hi Rob,

    Indeed. I put a 0.1uF capacitor blocking DC between the CDC device and the ADC. The common mode DC voltage is around 0.9V as expected.

    I replaced the ADC chip and it sprung into life. I must have had a dud, or accidentally hurt it at some point.... Thank you for your input it was very helpful.

    I have yet to try removing the capacitor and running the chip in single ended clock mode. Is there any reason why running with a single ended clock AC coupled into the chip would be bad? Effectively the common mode voltage of the clock is now being jerked around along with the clock.

    Will this alias to DC and degrade the ADC performance? As of now I appear to be seeing slightly more noise than advertised. (My application cares more about DC-fewMHz performance rather than pure spectral performance in the MHz).

    Best,

    Simon

  • Hi Simon,

    Its better to run the clock differential. From the schematic above it is being driving single-ended.

    If you are having noise issues, you need to first improve the clock performance, ie - lower phase noise/jitter, on the sampling clock.

    What is being used to clock the ADC, before the CDC device?

    Regards,

    Rob