Other Parts Discussed in Thread: ADS127L14, ADS127L11, ADS127L18, THS4551, THP210
Tool/software:
Hi, I am interested in lowest possible noise while maintaining sampling rate 50ksps or above. And for that I see the sweetspot is for my case sinc4 filter at OSR24 or 32, where at Fclk 25.6 or 32.768 MHz, the en noise is in 8.05 - 10.4uVrms range. I am referring here to the Table 6-2 of datasheet. I was checking the datasheet of another ADC AD4134 where I found interesting informationa about 2:1 / 4:1 channel averaging:
"The AD4134 is also capable of performing on-board averaging between two or four of its input channels. The result is a near 3 dB, if two channels are combined, or 6 dB, if all four channels
are combined, improvement in dynamic range while maintaining the bandwidth."
The relevant data for these settings are give in AD4134 datasheet table 13 and indeed the rms noise for 4:1 ch aveaging falls down to 4.66 uV.
ADS127L14/18 datasheet p. 63 also mentions that averaging, but no specs nor much details are given. Can you please help clarify this if, ADS127L14/18 , will give the same noise advantage of 6dB when doing 4:1 ch. averaging? And will it also maintaining the bandwidth? Are there other considerations when one tries to do channel averaging, particularty with sinc4 and OSR24/32 in the sweetspot I mentioned? Basically I want to use the ADC as single channel, at 500ksps but to get even lower uncorrelated noise (post-filter) than it has for sinc4 filter, while maintaining other specs.
By the way I am familiar with ADS127L11 - single channel version, I use its evaluation board and quite happy with performance.
Thanks in advance!
Karen