Part Number: TXB0104
Tool/software:
I need a level shifter to converter the Low Power Mode signal of MIPI DSI (1.2V at 10Mhz) to 2V or more
is TXB0104 up to the task? and what other options do I have?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXB0104
Tool/software:
I need a level shifter to converter the Low Power Mode signal of MIPI DSI (1.2V at 10Mhz) to 2V or more
is TXB0104 up to the task? and what other options do I have?
Hi Ossama,
From this previous thread, it seems to indicate that the MIPI DSI signals are fixed direction- can you confirm if this is also accurate to your use case as well? If so, devices like the AXC4T774 or TXU0x04 can be used to provide more robustness as the direction flow of the channel I/Os are fixed direction. Generally speaking, if your signals are not truly auto-bidirectional per channel, it is suggested to use fixed direction or direction controlled translators instead.
Regards,
Jack