This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8534: DAC: Inquiry

Part Number: DAC8534

Tool/software:

Dear Team,

I'm planning to design a RF board which need DAC ICs. Can you please suggest a DAC IC for my following requirement

2,4 or 8 channel
16 bit resolution
34 MSPS per channel
Each channel output upto +/- 1.85V for 1Kohm load
Ultra low latency
Ultra small glitch
THD less
1.2V and 1.8V logic compatible
2.5V internal voltage reference
form factor less than or equal to 5mm*5mm

Regards,

Abhishek