This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS9817: ADS981x Initialization - Data Sheet

Part Number: ADS9817

Tool/software:

Hello,

I saw from one answer about this issue that the first table in the data sheet ADS9817 (table 6-10) is the correct Initialization table.

If you look at the table it uses incompatible register addresses in several places. For instance, INIT_5 is set to '1' first at register 0x0A, the to '0' also at 0x0A. Later in the table it is again set to 0, but at register 0x13 (step number 13).

I assume; 

Step 9 is correct.

Step 13 sets INIT_3 to '0'? (should be register 0x12)

Step 14 sets INIT_4 to '0'? (should be register 0x13)

Are these a few more misprints? Thanks.

Mike

  • Hi Mike,

    Thanks for your post! The comments do look to be inconsistent in the initialization table, thanks for the note. But the actual register addresses and writes are correct and in the proper order. Please use the table addresses and writes as is.

    Additionally, if you are interested in the simultaneous sampling variant of this ADC, we do have it available now: ADS9813

    Best regards,

    Samiha