Other Parts Discussed in Thread: LMH5401
Tool/software:
I am using the original board using ADC32RF55.
After supplying power to the ADC on the board, I checked the VCM pin and found that 0 V was output.
Also, looking at the 0x298 register of the ADC, calibration failed.
When does the VCM pin start to output close to 0.35 V?
Also, does calibration need to be completed for the VCM to output 0.35 V?
Thank you and best regards,