This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3561: Parallel Port Check

Part Number: ADC3561

Tool/software:

Hi  TIer

My customer is looking for a ADC which is 10Msps 16bit or 18bit ADC with Parallel interface.

Do we have parallel interface version about ADC3561?

Thank you very much.

  • Hi Tony,

    Unfortunately, we don't have anything available that meets all the requirements, but we do have a few options below:

    ADC3541 Parallel CMOS interface but only 14 bit resolution

    ADS9813 can run in oversampling mode to have 2 channels running at 8MSPS each

    ADS5560 older 16 bit ADC with parallel CMOS interface. Has a low-speed mode that can run the ADC from 1-25MSPS.