Tool/software:
Hello, I wanted to confirm if to synchronize multiple ADC3544s the sync signal has to have a specific frequency/phase. That is to say, does the sync frequency have to match the input clock frequency, be a multiple of it, or be phase locked to the external input clock signal? And is there a maximum/minimum frequency for the sync signal?
I am attempting to synchronize multiple devices using the ADC3544 with a GPS pps signal, or derived GPS disciplined clock to feed into the ADC sync lines. Thank you!