Part Number: DAC8750
Tool/software:
Dear TI team,
please have a look at the schematic snippet.

In our design the +12V power rail is not continuously switched on, while the 3V2 power rail is always on.
If the +12V power rail is switched on, the voltage nDACALM is about 3,2V as expected, given the *ALARM pin of DAC8750 is inactive/high impedance.
If the +12V power rail is switched off (left floating), the voltage at +12V decreases to about 2,0V (due to some leakage currents in other parts of the design), and the voltage at nDACALM decreases to about 2,65V.
If the +12V power rail is switched off and shorted to ground, the voltage at nDACALM is pulled down to approx. 650mV.
This lets us assume that the *ALARM pin of DAC8750 surprisingly is clamped by a pn diode to AVDD instead of DVDD.
Two questions arise:
- Is the assumption concerning the clamping right?
- More important: Is it safe to have some current flow from *ALARM pin to AVDD pin of DAC8750?
Best regards
Rainer