This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS127L18: Datasheet clarification: Start/Stop Control Mode

Part Number: ADS127L18

Tool/software:

Hi team,

There is a question about 7.4.5.2 Start/Stop Control Mode of ADS127L18 DS-ADC.

This is the diagram in the data sheet.

 

The question is what happens at the START pin when it goes HIGH again after being LOW?

  1. The ADC starts again with Filter Latency,
  2. OR, The ADC starts again without the Filter Latency.

Which one is the correct operation?

If the answer is 2), then the next FSYNC rising edge, will it be n-th FSYNC delay or related to the time of the rising edge of START?

Best regards,

Randy

  • Hello Randy,

    The ADC conversion restarts with the filter latency (1. The ADC starts again with Filter Latency)  

    If there is a conversion still in process on START rising edge, then the current conversion will be reset (lost) and the new conversion will start (FSYNC will be forced low if not already low).  After the filter latency period, FSYNC will go high indicating new conversion data are being clocked.

    If there is no conversion in process (FSYNC is low), then you will start a new conversion and FSYNC will remain low for the filter latency period.