Tool/software:
Hi team,
There is a question about 7.4.5.2 Start/Stop Control Mode of ADS127L18 DS-ADC.
This is the diagram in the data sheet.
The question is what happens at the START pin when it goes HIGH again after being LOW?
- The ADC starts again with Filter Latency,
- OR, The ADC starts again without the Filter Latency.
Which one is the correct operation?
If the answer is 2), then the next FSYNC rising edge, will it be n-th FSYNC delay or related to the time of the rising edge of START?
Best regards,
Randy