ADC3910S025: vcm impedance, data alignment

Part Number: ADC3910S025


Tool/software:

What is the output impedance/current drive capability of the Vcm output?

I assume I can ignore the SPI interface, hardware reset it, and use it as a plain 10-bit parallel ADC, in its default mode. Is that OK?

If so, where do the 10 data bits come out? There are 12 pins, D0 through D11.