Other Parts Discussed in Thread: ADS1298, ADS1298RECGFE-PDK, ADS1298R
Hello,
We purchased the ADS1298RECG-pdk evaluation development kit and noticed that an executable(ADS1298e.exe)came with it. Additionally, it
would seem that the executable was developed from labview.
I looked into the folder where the application is installed and notice that there are VIs located throughout the installed folder. I have tried
to match the ADS1298E.exe's GUI application with the accompanied Vis and wasn't
able to do so.
Are the ADS1298E.exe's VIs located in the extracted folder and if so can what are their file names?
If not can where can I get the VIs that were used to create the ADS1298.exe.
Thanks Very Much.
--cat--