ADC12DJ5200-SEP: ADC12DJ5200 - NCO Phase Synchonization Time

Part Number: ADC12DJ5200-SEP

Tool/software:

Hello,

I understand that TI has responded that approximately 200ms is required for calibration when changing to JESD mode.

I have the following questions:

1. What is the approximate time required for NCO Phase Synchronization described in the datasheet section 6.3.8.2.6?

2. Does the time depend on the SYNC being set 'High' when NCO Phase Synchronization is completed?

3. Can the 'NCO Phase Synchronization' time be calculated using the timing requirements tH and tSU in section 5.9?

Best regards,

Young Jun.