Part Number: DAC80502-01EVM
Other Parts Discussed in Thread: DAC80502, , DAC80501
Tool/software:
Hello,
I'm testing DAC80501 and DAC80502 on DAC80502-01EVM.
I found the DACs don't work when the VDD is 3.3V by VDD-SEL jumper.
Using external VDD, decrease the VDD from 5.0V, the DAC output level shuts down to 0V when the VDD is 3.60V.
If I increase the VDD voltage, the output goes back. The VREF voltage is stable until VDD = 2.6V. The GAIN setting didn't affect the behavior.
Could anyone please provide some advice? Our application uses 3.3V VDD, and it is an important problem.
Best Regards,