This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Some questions on hardware design and operation

Part Number: DDS39RFS10
Other Parts Discussed in Thread: LMX2592, , TPS7A94, TPS7A15, TPS7N53, TPS62913

Tool/software:

Planning to use DDS39RFS10 in DDS only mode w/ DES (both DES2XL and DES2XH). Clocked with LMX2592 at ~7.1 GHz Fclk. Need some clarification on these points.

5. Is <1 µVrms noise LDO (TPS7A94) essential or would anything below 10µV be good enough for VDDCLK10 and other sensitive rails? LDOs like TPS7A15 / TPS7A14 would allow for 1.2V -> 1.0V

8. Would the TCM2-722X+ balun work fine for the outputs? The eval board sch used a 3 dB T-attenuator (but 50 Ohm impedance?), is this necessary when the balun is well-matched? Or is the DAC output itself not a perfect 100ohm diff? S-parameters would help here.