This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF82EVM: DAC38RF82EVM ZCU111 integration

Part Number: DAC38RF82EVM


Tool/software:

Hello Everyone, 

I have a quite expensive ZCU111 FPGA board and do not want to invest more into another FPGA board and would like to evaluate DAC38RF82EVM with this board. I already have a pin comparison and seems to be mostly matching except SYNC pins (not connected in ZCU111 board).

Could you please guide me to quickest bring-up path that is kind of proven to work? 

If you have a reference design for example using ZCU102 or similar board, would be great. Also would be very helpful if there are any designs including the Zynq Ultrascale+ PS subsystem to program and control the overall design (SPIs etc.)

I also started to look into the TI_204c_IP reference designs but they seem to be more generic rather than specific to any Data Converter. Still would try to use that as well if you could help me on the required connections and settings for DAC38RF82EVM.

Depending on the progress I need to decide to buy or not DAC38RF82EVM board (compatibility to ZCU111/ZCU102).

I would appreciate any help.

Regards,

Ömer.