ADC0820-N: Questions about the material/qual of this part

Part Number: ADC0820-N

Tool/software:

 Hi all-

Can you provide answers to these questions below?

  1. Is the part sensitive to the following solutions or solvents?
    1. Acetone
    2. IPA
    3. MEK
    4. Toluene
    5. Water, All Types
    6. Axarel 2200
    7. Petroferm Bioact EC-7R
    8. Kyzen Ionox 13330
    9. Kyzen Booster 20
    10. Micro Care Proclean
    11. TDS Quanox A4630
    12. Dupont Vertrel SFR
    13. Vigon A201

 

  1. Is Pre-Heating required before hand installing the part?

 

  1. What is the maximum ramp rate the part can be subjected to without physically and/or functionally degrading the part?

 

  1. If reflow is used, will the part be physically and/or functionally degraded when exposed to a ramp rate of four (4) degrees (Celsius) per second?

 

  1. Does the part have a moisture sensitive rating in accordance with J-STD-020?

 

Thanks,
Lauren