ADC3663EVM: ADC3663EVM

Part Number: ADC3663EVM
Other Parts Discussed in Thread: ADS9219EVM

Tool/software:

Hello,

Evaluating ADCs for a new design and I would like to know if i can interface directly the ADC3663EVM with a Xilinx AC701 Eval board. 

From the ADC3663EVM schematic (DC134, REV E), I see that the FMC H2 signal is grounded which disconnects the JTAG TDO signal on the AC701 but the signals D30/31 are tied together which should solve the JTAG problem. Is that correct? and if it is that would mean that I could use my AC701 board to interface with your ADC3663EVM board, correct? 

Another option was the ADS9219EVM, but it was pointed out in the forum that JTAG problem with another Xilinx Eval Board KC705. Is that going to be fix in a new ADS9219EVM revision?

Thanks,

Jose Berroteran