This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS9219EVM: ADS9219EVM

Part Number: ADS9219EVM

Tool/software:

xtp078.pdf

Evaluating ADCs for a new design and I just would like to confirm that i can interface the Xilinx FMC XM105 debug bug537.pdfoard with the ADS9219EVM since i cant interface directly with the Xilinx AC701 board without modifications as pointed here:  ADS9219EVM: wrong schematic related to JTAG .

Thanks

Jose Berroteran

  • Hello Jose, 

    Yes, the Xilinx FMC XM105 debug board does bring out all the required pins to use with the ADS9219EVM 

    The only concern is the "SMPL_SYNC" pin that uses the LA32_P which is tied to an LED on the debug board. This can just be mitigated on the EVM board with JP4.

    Best regards,

    Yolanda