This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC3283: DAC3283: Design Inquiry

Part Number: DAC3283

Tool/software:

Hi Team,

My board clock requirement block diagram is attached below.

The clock from the clock synthesizer need to feed as input clock to all ADC, DAC and FPGA in the board to make a synchronization.

Also from FPGA an input SYNC IN/ LDAC like input signal is fed to all the ADCs and DACs so that FPGA can control and sync activities of all the data converters.

My DAC required output range is +/-1.85V.

Can i use the DAC3283 for my application.

If yes please suggest an output buffer amplifier to DAC IC so that i need a single ended output to be connected to a SMA connector.

Please provide an update on above mentioned query.

Regards,

Abhishek