Other Parts Discussed in Thread: ADS1293
Tool/software:
Hello,
I recently purchased two ADS1293EVM evaluation boards, but both are not detected by the ADS1293 GUI software. When I launch the application, it shows the error message “No Board Found – Number of boards: 0” (see attached screenshot).
Here are the details:
- GUI Version: ADS1293EVM GUI v1.0.0
- DLL Version: 2.0.0 (build 6)
- OS: Windows 10 64-bit
- The LED on the board does not light up when connected via USB
- I already tried several USB cables and ports
- The driver does not appear in Device Manager (no MSP430 or TI interface)
- I installed the GUI as administrator and also reinstalled the TI USB drivers, but still no detection.
Could you please help me understand:
1. Which USB driver or firmware is required for proper communication between the ADS1293EVM and the GUI?
2. How can I verify if the MSP430 is correctly programmed on the board?
3. Is there a way to manually flash the firmware or update the USB interface?
Thank you in advance for your support.
Best regards,