Part Number: ADS9219
Hi Team,
We have an application where 7 ADS9219 devices will work synchronized by the same SMPL_CLK signal (20MHz).
The data averaging mode will be activated with the averaging set to 2 (probably). We will use the SMPL_SYNC input in order to syncronize the ADCs (one general sync pulse applied at ADC init)
For each ADC we intend to use 2 lanes of data (DOUTA + DOUTB).
Our expected DCLK frequency will be:
fDCLK=20MHz*24bits_frame/(2 (avg)*2(data_lanes)*2(DDR))= 60MHz
We are short in FPGA available pins.
So the questions are:
1. Considering the fact that the ADCs are syncronized can we use a single DCLK LVDS lane for all the 7 ADCs?
2. Applying a single synchronization pulse at init is to ensure syncronization during ADCs operation or multple/repeated SMPL_SYNC pulses are requested?
3. Can we avoid connecting the FCLK signal at all? Since the FPGA is generating the SMPL_CLK signal and since the FPGA is clocked at 100MHz or even 200MHz we would like to emulate internally FCLK in order to spare some I/Os.
Some example code/application notes will be warmly welcomed :). The FPGA is an AMD one.
Best Regards,