Hello,
At AMC87208, is it possible to OR multiple IDAC# pins to get larger output current?
Best regards,
K.Hirano
Hi Hirano-san,
You can connect multiple IDAC outputs together in parallel for increased current. One general comment when doing that: we recommend that the channels are all set to the same value to help distribute power dissipation in the die. For example, if you have 2 channels in parallel and want a combined current of 200mA, we recommend each channel contribute 100mA. That way the load is evenly distributed.
Thanks,
Paul