Other Parts Discussed in Thread: ADS1298, ADS1294
Hi Team,
The recommended capacitor value for VCAP1 in ADS1299 is 100uF and the internal resistor R1 is 9.8kOhms which takes around ~2.4sec for the Vcap1 to reach 1.1V.
- I wanted to know if the wait time until VCAP1 reaches >1.1V as per the the initial flow is really necessary if we are using the external reference?
- What is the consequence if we do not wait until this time under both conditions mentioned below?
- While using internal reference
- While using external reference
- Is the consequence same in ADS1298/6/4 ?
Thank you in advance.