How shall unused parallel lines (Dx) be handled if ADC is configured in serial mode? Datasheet (SBAS905C) says : "In serial mode, these pins must be connected to DGND." (e.g. for DB0, 1, 2 3 on page 4). The question raised up, since DBx pins are of DIO type. Is there a possibility that the pins are actively driven even if ADC is configured in Serial Mode (SER/PAR* tied to +3.3V).
Q1: Can we directly tie the pins to DGND without any series resistors?
Q2: If for safe operation resistors are required: what is the proposed value range?