This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3664EVM: Can't connect to ADC3664EVM by ADC36xxEVM GUI.

Part Number: ADC3664EVM
Other Parts Discussed in Thread: ADC3669, ADC3669EVM, TSWDC155EVM

Hi

I can't connect to ADC3664EVM by ADC36xxEVM GUI.

Please teach me how to use.

Conditions,
--Connect PC and A via USB cable
--Input 12V from DC jack
--Verify ADC3664EVM USB LED is lit
--Verify ADC3664EVM Power LED is lit

 

After confirming the above, launching the ADC36xxEVM GUI results in an error as shown in the image.

image.png

Checking Device Manager shows USB recognition as follows:

image.png

It seems like an FX3 USB driver error.

I uninstalled and reinstalled the ADC36xxEVM GUI, but the same issue persists.

What could be wrong?

Best Regards,Kato