This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC0800: DAC Selection

Part Number: DAC0800

Hello E2E Experts,

I have two DAC implementations which I would like to consult on:

  1. Using a current output DAC that has a fast-setting time, has a parallel input, at least a 12-bit accuracy and monotonic. This is for a DC application.  The full-scale DC current should be at least 12ma.  Since this is for DC applications, a strobe, not a clock would be used.
  2. DAC will be used for DDS applications.  Sampling frequency will be 166 2/3MHz, Needs to have a parallel interface, at least 14-bit accuracy (80dB SFDR with an output around 80MHz, 166 2/3 clock), and a fast input to output settling time.

Both should have a small footprint and as low power consumption as possible.