Part Number: ADC3908D125
Hello E2E Experts,
We are feeding a 250mV signal into the inverting input of the AD8002. The single-ended output (Gain=1) from the AD8002 is then connected to the non-inverting input of the AD8138. The differential outputs with swing (1.9Vp-p) from the AD8138 are fed into the ADC3908D125, and the 8-bit outputs from the ADC are sent to the FPGA.
as we did simulation for cascaded AD8002 & AD8138 and got the differential swing approximately 1.9Vp-p, Could you please give us the guidance to simulate ADC3908D125.